Skip to main content
Ey.1
Associate II
Feb 22, 2021 4:15 PM UTC
Question

STM32H743 Using of Multichannel ADC Triggered by Timer in Interrupt Mode

I'm having a trouble when using multichannel ADC. In my application there is 2 ADC which contains 7 channels. In ADC Interrupt Callback, I'm pushing the read data to array of 7 elements. But I couldn't see the proper value in proper element of array, they are sliding in the array countinously.

Each ADC contain seven ACS725. So there is no High-Z situation. I'm seeing at the pins 0.5V constant (zero current) . My callback and init part is in above. Thanks a lot for your help!

/* ADC3 init function */
void MX_ADC3_Init(void)
{
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /** Common config
 */
 hadc3.Instance = ADC3;
 hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV4;
 hadc3.Init.Resolution = ADC_RESOLUTION_16B;
 hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc3.Init.LowPowerAutoWait = DISABLE;
 hadc3.Init.ContinuousConvMode = DISABLE;
 hadc3.Init.NbrOfConversion = 7;
 hadc3.Init.DiscontinuousConvMode = DISABLE;
 hadc3.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T15_TRGO;
 hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
 hadc3.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc3.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc3) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_REGULAR_RANK_4;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_6;
 sConfig.Rank = ADC_REGULAR_RANK_5;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_7;
 sConfig.Rank = ADC_REGULAR_RANK_6;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_8;
 sConfig.Rank = ADC_REGULAR_RANK_7;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
	if(__HAL_ADC_GET_FLAG(&hadc1, ADC_FLAG_EOC))
	{
		g_internalAdc1.m_rawResultArray[cntAcs1++] = (uint16_t) HAL_ADC_GetValue(hadc);
 
		if(cntAcs1 == g_internalAdc1.MS_NUMBER_OF_CHANNEL)
		{
			cntAcs1 = 0;
			g_internalAdc1Ready = true;
		}
	}
 
	if(__HAL_ADC_GET_FLAG(&hadc3, ADC_FLAG_EOC))
	{
		g_internalAdc2.m_rawResultArray[cntAcs2++] = (uint16_t) HAL_ADC_GetValue(hadc);
 
		if(cntAcs2 == g_internalAdc2.MS_NUMBER_OF_CHANNEL)
		{
			cntAcs2 = 0;
			g_internalAdc2Ready = true;
		}
	}
}

In SystemClock_Config function:

PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL3; //129Mhz ( (I also tried other options)

My timer also adjusted to 40ms period.

In debug, what I mean results are sliding in the array :

0693W000007Z7HqQAK.png 

0693W000007Z7IFQA0.png 

etc...

(while ~7000 raw data is zero current, ~14000 is equalt to 1.2 Amper. I'm applying the 1.2A to only one channel that has to be in the 3rd element of the array)

After I tried with a new project with applying same configurations with using only 2 channel: I aware that there is only 1 conversion result. The other result does not seen on the callback and also DR register. And when I start the ADC with software(without timer trig) it looks like it takes the result from random channel. I could not solve problem for three days.

Thanks again.

This topic has been closed for replies.

4 replies

Vangelis Fortounas
Associate II
Feb 22, 2021 7:49 PM UTC

Hello

ADC1 and ADC3 have different IRQ handlers and different NVIC priorities (one interrupts the other)

Inside completion_callback dont check for eof flag.

Check the handle

if(hadc==&hadc1) {;}

else if (hadc==&hadc3)

else{;} //whatelse

The Fadc is about 32Mhz .Is BOOST bit(s) set? (boost functionality differentiates with chip revision Y or V)

0693W000007Z8hpQAC.jpg 

0693W000007Z8qwQAC.jpg

Ey.1
Ey.1Author
Associate II
Feb 23, 2021 8:23 AM UTC

Thanks for reply! I changed the conditions in callback like you say. I was not aware of boost mode, it was on reset state. My chip is V revision, and I set the these two bits and I also observe in SFRs they changed to true state. But there is no timing differences.

Ey.1
Ey.1Author
Associate II
Feb 23, 2021 10:05 AM UTC

When in continuous mode, disabling the timer trigger, values always sliding in the array :(

Ey.1
Ey.1Author
Associate II
Feb 25, 2021 7:19 AM UTC

In DMA mode, disabling adc global interrupt, it is working in a true way. But in interrupt mode, I could not handle.