Skip to main content
Visitor II
Jan 16, 2026 7:01 PM UTC
Solved

STM32H743 triggers multiple NWE for single write in FMC

Im trying to drive 3.5 inch TFT LCD with STM32H743 using FMC. My setup is :

  • ChipSelect: NE1
  • Memory Type: LCD Interface
  • LCD Register Select: A18
  • Data: 8 Bits

My timing settings are (FMC Clock: 10Mhz): 

  • Address setup time in FMC clock: 3
  • Data setup time in FMC clock: 2
  • Bus Turn around time in FMC clock: 2

Here are the parts of code:

  • #define FMC_BASE ((uint32_t)0x60000000)
  • #define LCD_CMD (*((volatile uint32_t *)(FMC_BASE)))
  • #define LCD_DATA (*((volatile uint32_t *)(FMC_BASE | (1 << 18))))

When I try to write a data, as shown in the attachment, my logic analyzer shows me multiple WR event occured and shows some weird signals on data line (D0-D3).

I do not understand where I did wrong...

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 17, 2026 9:12 PM UTC

Hello,

To drive LCDs through FMC with MCUs with Cortex-M7 you need to configure the LCD memory region in Strongly-Ordered or Device configuration using the MPU.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 17, 2026 9:12 PM UTC

Hello,

To drive LCDs through FMC with MCUs with Cortex-M7 you need to configure the LCD memory region in Strongly-Ordered or Device configuration using the MPU.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.