Skip to main content
ST Migration account
ST Community Manager
Aug 22, 2026 5:02 PM UTC
Solved

STM32H743 trigger SPI transfer via Timer

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.


I am currently struggling to figure out if my current requirents are even possible.

I am building a network controller to controll laser projectors via analog lines.

For that I have an DAC8552 connected to SPI1 and a DAC1240S85 connected to SPI2.

The way I control SPI1 & SPI2 is almost identical so I will focus on SPI1 for now.

I have the following requirements:

  • 200k times per second (200kHz) I need 3 bytes being transferred via SPI
  • right before and during that transfer an LDAC line needs to be asserted low and afterwards it needs to be brought back up. This is important for the DAC to actually latch the bits
  • The timing is critical and must be precise and each transfer must happen within its 5uS timeframe including the LDAC assertion and deassertion.
  • I can't have any CPU involvement besides feeding some sort of DMA a new buffer as I also handle Ethernet with LwIP, decoding the network packages and have to do the same with 4 packages later on on SPI2.

My favorite idea so far is to use a timer like TIM3 and generate a PWM signal to produce an LDAC signal on one channel and then trigger an SPI transaction on CH2.

But it really doesn't seem like there is a way to do that.
Since the LDAC line and the SPI clock must be pretty syncronized when an SPI-Byte is being transferred I don't se a way where I can simply keep my SPI being feed with dummy-data by DMA.

I am getting that desperate that I'm actually trying to see if I can exploit the SPI running dry and spoonfeeding it by triggering DMA transfers into it's TX-Fifo.

But would that even work?

 

There must be a way to properly time and automatically trigger SPI transactions on STM32H7 or am I completely missing the point?

If an answer needs more information or more precise requirements I'm fast to answer

MasterT
MasterTBest answer
Lead II
Aug 22, 2026 5:06 PM UTC

 wrote:

My favorite idea so far is to use a timer like TIM3 and generate a PWM signal to produce an LDAC signal on one channel and then trigger an SPI transaction on CH2.

 Seems right, trigger DMA transaction to SPI-DR and sync LDAC by another channel of timer. Configure SPI clock fast enough to complete data transfer in time.

SPI doesn't have to be synchronous, since update event of the DAC is strictly defined by timer. SPI transfer may drift/ jitter in the LDAC's window but it does not matter.

3 replies

MasterT
MasterTBest answer
Lead II
Aug 22, 2026 5:06 PM UTC

 wrote:

My favorite idea so far is to use a timer like TIM3 and generate a PWM signal to produce an LDAC signal on one channel and then trigger an SPI transaction on CH2.

 Seems right, trigger DMA transaction to SPI-DR and sync LDAC by another channel of timer. Configure SPI clock fast enough to complete data transfer in time.

SPI doesn't have to be synchronous, since update event of the DAC is strictly defined by timer. SPI transfer may drift/ jitter in the LDAC's window but it does not matter.

ST Migration account
ST Community Manager
Aug 22, 2026 5:09 PM UTC

Thank you, I can see that to feed the SPI-DR via DMA triggered by Timer.

Do I keep my SPI constantly transmitting so it runs dry between the individual transfers before another DMA transaction feeds it another 3 bytes?

For that I imagine setting up my SPI to transmit buffer-length many bytes in total and restart that transmission whenever a DMA buffer gets refreshed.

Or is there a way to basically tell the SPI "Clock out whatever you get in on TXDR as soon as you can"?

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
MasterT
Lead II
Aug 22, 2026 5:10 PM UTC

It's done by hardware in automatic, SPI starts transmission as soon as DMA puts data to SRI-DR, than SPI stops and waiting another portion of data.