Question
STM32H743 : Reading UART7 while writing on UART4
Hello, I have issues with STM32H743 UART. I use Nucleo 144 and I need to get GPS frames on UART7 (at 9600 baud) and display them on UART4 (at 115200 baud). If nothing is sent on UART4, reception of frames on UART7 is good but I want to display some values at the same time on UART4. If I do that, the frames on UART7 are not entirely received, some caracters are missing. More I print values on UART4 more there are missing caracters on UART7. Is that normal ? What can I do about this ? Thanks for your help !