Skip to main content
lucky65
Associate II
Jun 10, 2025 11:38 AM UTC
Solved

STM32H743: QUADSPI internal timing criticality errata

Hi all,
I am working on a QSPI driver for W25Q512 flash memory (extloader for stm32cubeprogrammer and main firmware driver).

I had a look at the errata ES0392 - Rev 13 and I have a question about paragraph 2.8.4:

2.8.4 - QUADSPI internal timing criticality
---------------
Description
The timing of some internal signals of the QUADSPI peripheral is critical. 
At certain conditions, this can lead to a general failure of the peripheral. 
As these conditions cannot be exactly determined, it is recommended to systematically apply the workaround as described.
...
[omissis]

 

I have applied the suggested patch on the "external loader" driver and there is no particular problem in applying it,  but I have also the "very similar" driver on the main application firmware in processor.

 

Up to now I had no errors in the main firmware qspi driver : read and write are ok also without the patch.

 

Applying the patch on the "main firmware" needs testing and I have to schedule this testing.

Is it possible to have some more details on this "certain conditions" to better evaluate the situation and get less worried about this... ?

Does it mean clock, temperature, ...?

 

Thanks,

best regards

 

Lucio

 

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 24, 2025 11:28 AM UTC

Hello,

According to our expert, unfortunately we don't have the exact condition when the issue could happen. It could be the clock, temperature, voltage ... It's linked to a synchronization issue between two clock domains that could be influenced by temperature, clocks, voltage ..

So in any case you need to apply the workaround.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

mƎALLEm
ST Technical Moderator
Jun 10, 2025 1:25 PM UTC

Hello,

I will check internally and get back to you as soon as I have an answer.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 24, 2025 11:28 AM UTC

Hello,

According to our expert, unfortunately we don't have the exact condition when the issue could happen. It could be the clock, temperature, voltage ... It's linked to a synchronization issue between two clock domains that could be influenced by temperature, clocks, voltage ..

So in any case you need to apply the workaround.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
lucky65
lucky65Author
Associate II
Jul 11, 2025 10:15 AM UTC

Hi,

sorry for my late reply.

I applied the suggested workaround ; thanks a lot for your answer .

 

Best regards,

Lucio