STM32H743 jumping to wrong interrupt when I move the vector table when using LPUART
I have an application using STM32H743 we wish to use the LPUART using the interrupt. We have a bootloader that is located 0x08000000 until 0x08020200. According to system_stm32h7xx.c we should move the vector table in steps of 0x200 this works for all of our interrupts apart from LPUART.
I have used cube MX to generate a new test project that just enables the LPUART and only has 1 line that send data HAL_UART_Transmit(&hlpuart1,TestData,9,1000); It also crashes. But is the code works if the start is at 0x8020000 or 0x8020400. I have tried 0x8020100 and 0x8020300 they do not work.
Is system_32h7xx.c wrong and the vector table should be in steps of 0x400?