Skip to main content
Gabriel Gagnon
Associate
October 13, 2020
Question

STM32H743 IWDG Standby

Hi,

I have been banging my head for a while now and decided to reach out for help. I am trying to get the IWDG to freeze during Standby. Based off the reference manual I have toggled the IWDG_FZ_SDBY bit to 0. In STM32CubeProgrammer it is set to 0 so theoretically it should Stop the IWDG while in Standby. But the board keeps resetting, I decided to test this out on the NUCLEO-H743ZI2, same thing is happening and the code is extremely simple.

HAL_Init();
SystemClock_Config();
 
FLASH_OBProgramInitTypeDef OBInit;
HAL_FLASHEx_OBGetConfig(&OBInit);
if(OBInit.USERConfig & OB_IWDG_STDBY_ACTIVE)
{
	// Unlock flash option bytes
	HAL_FLASH_Unlock();
	HAL_FLASH_OB_Unlock();
 
	OBInit.OptionType = OPTIONBYTE_USER;
	OBInit.USERConfig = OB_IWDG_STDBY_FREEZE;
	OBInit.USERType = OB_USER_IWDG_STDBY;
	HAL_FLASHEx_OBProgram(&OBInit);
 
	HAL_FLASH_OB_Launch();
}
 
 MX_GPIO_Init();
 MX_ETH_Init();
 MX_USART3_UART_Init();
 MX_USB_OTG_FS_PCD_Init();
 MX_IWDG1_Init();
 
 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, SET);
 int i =0;
 
while (1)
{
	HAL_Delay(300);
	HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
	i++;
 
	if(i>=10)
		HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, RESET);
	if(i>=30)
	{
		__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
		HAL_PWR_EnterSTANDBYMode();
	}
	HAL_IWDG_Refresh(&hiwdg1);
}

I also tried the same thing on the NUCLEO-L432KC and this time it is working. I have looked online to see if people had a similar problem and cannot seem to find anything about this.

Anyone can help?

I will be implementing a quick solution in the meanwhile that includes writing to the flash before going in Standby and reading that flash at boot. I would prefer not use this in the final product though.

Thanks

This topic has been closed for replies.

2 replies

Associate
April 25, 2024

hi Gagnon. have you figure out the reason why the board keeping reseting after enter Standby Mode?

i get the same issue.

Dams
Associate III
October 24, 2024

Hello, 

I have the same behavior with a STM32H725 but only on debug session (no matter the configuration of the debugger about the option "suspend watchdog while halted").
The MCU works well when there is no debug session (MCU start from a power on).
Hope this can help you.