Skip to main content
Handzic.Dirk
Associate III
May 24, 2018
Question

STM32H743 errata

Posted on May 24, 2018 at 12:03

I have designed a board using the STM32H743II. During integration testing of the software I have found the following issues related to the microcontroller (SCB->CPUID 0x411fc271) :

1)SPI1 and ADC1 is not working when using PLL2 P output due to the bit DIVP2EN in RCC_PLLCFGR stuck at '0'. This is probably true for all peripherals which could use PLL2 output P. PLL3 output P works fine as clocksource.

2)ADC1 is not working when using PLL3 R output due to the bit DIVR3EN in RCC_PLLCFGR stuck at '0'. This is probably true for all peripherals which could use PLL3 output R. PERCLK works fine as ADC1 clock source,

3) TIM2->ARR is 0x00000000 after reset NOT as in the RM 0xFFFFFFFF and will not start counting even when configured as up counter as long as ARR is 0x00000000 (which is not outlined in the RM either). Thanks Jan Waclawek for the help!

Hopefully this will spare other developers some time. I spent a couple of days on it before I found the reason and a solution.

Best regards

Dirk

This topic has been closed for replies.

10 replies

Amel NASRI
ST Technical Moderator
May 25, 2018

Posted on May 25, 2018 at 13:26

Hi

Handzic.Dirk

‌,

1)SPI1 and ADC1 is not working when using PLL2 P output due to the bit DIVP2EN in RCC_PLLCFGR stuck at '0'. This is probably true for all peripherals which could use PLL2 output P. PLL3 output P works fine as clocksource.

==> Is there any other peripheral using PLL2Q or PLL2R?

2)ADC1 is not working when using PLL3 R output due to the bit DIVR3EN in RCC_PLLCFGR stuck at '0'. This is probably true for all peripherals which could use PLL3 output R. PERCLK works fine as ADC1 clock source,

==> Is there any other peripheral using PLL3P or PLL3Q?

In fact there is an issue with RCC driver in the STM32CubeH7 package when using more than one output on PLL2 or PLL3 as clock source for 2 or more peripherals. A patch is developped and should be deployed in coming release of the package.

Please let me know if you would like to test this patch in order to confirm if this is really the root cause of the issue or not.

3) TIM2->ARR is 0x00000000 after reset NOT as in the RM 0xFFFFFFFF and will not start counting even when configured as up counter as long as ARR is 0x00000000 (which is not outlined in the RM either). Thanks Jan Waclawek for the help!

==> I suggest to follow this problem in 

https://community.st.com/s/feed/0D50X00009XkZJuSAN

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
May 25, 2018
Posted on May 25, 2018 at 14:34

>>Please let me know if you would like to test this patch in order to confirm if this is really the root cause of the issue or not.

Yes, I'd like whatever patched RCC code you can supply, issues here can be particularly difficult to understand, and the clock routing on the H7 is complex/critcal. The issues with SDMMC clocks also stem from the PLL configuration modes and interactions. The Peripheral Clock HAL code strikes me as rather confusing.

Also can someone please refactor to the Get PLL functions so they don't read the same PLL/RCC registers a dozen times, these registers are 'volatile' and the compile cannot optimize this code. Take a snap shot of the value into a local copy and process that.

Example for F7 PLL decoder

https://community.st.com/0D50X00009Xki9ZSAR

I have something similar for the H7, search isn't helping me right now, will find again later

Ok, this thread, it uses the ST functions I think need refactoring

https://community.st.com/0D50X00009XkhUQSAZ

I find that I need to write these clock decoder/cracking routines to I can understand what's going on internally.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Technical Moderator
May 25, 2018
Posted on May 25, 2018 at 17:10

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6uG&d=%2Fa%2F0X0000000bxk%2F65ghTvVQKhEXjiRv5.bEHmOD6xTF0U50gwzQlJ2RxbI&asPdf=false
To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Torsten Jaekel
Associate III
June 21, 2018
Posted on June 21, 2018 at 20:52

WHAUUU - GREAT - it works with this fix:

now I can use PLL2 for SDMMC and also PLL3 for USB plus I2C - all works fine now.

Thank you.

BTW:

don't forget to modify the prototypes:

//ERRATA

static HAL_StatusTypeDef RCCEx_PLL2_Config(RCC_PLL2InitTypeDef *pll2, uint32_t Divider);

static HAL_StatusTypeDef RCCEx_PLL3_Config(RCC_PLL3InitTypeDef *pll3, uint32_t Divider);
Amel NASRI
ST Technical Moderator
July 26, 2018

Fix deployed in STM32CubeH7 v1.3.0 currently available on the web.

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
T J
Senior III
September 2, 2018

what was the actual fix ?

check to see if DIVP2EN is set ?

after you run __HAL_RCC_PLL2CLKOUT_ENABLE(RCC_PLL2_DIVP); ?

but ?

As far as I could see it is just impossible to set the DIVP2EN bit even using a statement as *(__IO uint32_t *) 0x5802442C |= 0x00080000 would not set the bit.

in the IOC cube file;

I have change the PLL clock routing in order to run the SPI1 and ADC1 correctly.

(this file is not attached)

@Amel NASRI​ 

The following parameters cannot be changed after the PLL is enabled: 
DIVNx,PLLxRGE, PLLxVCOSEL, DIVPx, DIVQx, DIVRx,DIVPxEN, DIVQxEN, DIVRxEN.

Vanh
Associate
March 25, 2019

For me, when using SPI (Full-Duplex Slave) mode, if I set (Hardware NSS input signal), the spi does not work, I have to disable it and it operated, does anyone encounter like me