Skip to main content
Visitor
Jul 17, 2026 6:01 AM UTC
Solved

STM32H743: does this MCU support MIPI LCD?

Can connect STM32H743 with LCD with MIPI interface ?

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 17, 2026 6:43 AM UTC

Hello ​@Robinson2007 and welcome to the ST community.

The answer is No. It supports only LTDC interface with no MIPI-DSI host.

If you need a STM32H7 with MIPI interface. You need to select one of the dual core Graphical line products: STM32H747 or STM32H757.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 17, 2026 6:43 AM UTC

Hello ​@Robinson2007 and welcome to the ST community.

The answer is No. It supports only LTDC interface with no MIPI-DSI host.

If you need a STM32H7 with MIPI interface. You need to select one of the dual core Graphical line products: STM32H747 or STM32H757.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.