Skip to main content
Associate III
Feb 14, 2025 6:32 PM UTC
Solved

STM32H733 data cache initialization issue

Hello,

I am using a STM32H733VGT on a custom design board. On a fresh project in CubeMX, I tried to activate data cache but the autogenerated code crashes at  SCB_EnableDCache(); . (nothing has been activated on the CubeMX, just the external crystal and debugging port)

i tried enabling or disabling MPU as well, same results.

I need data cache for activating ethernet.

 

Any help would be highly appreciated.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 18, 2025 11:00 AM UTC

Hello,

I didn't find that exact device STM32H733VGT but tested your ioc file on NUCLEO-H723ZI board (STM32H723ZI) and I didn't reproduce the behavior.

Don't step into SCB_EnableICache() and SCB_EnableDCache().

If you put a break point on HAL_Init() and run, do you reach it? 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

9 replies

mƎALLEm
ST Technical Moderator
Feb 14, 2025 6:35 PM UTC

Hello,

Are you sure you've generated a project for STM32H733 and not another MCU device?

Is that possible to share your ioc file?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
amirshnAuthor
Associate III
Feb 14, 2025 6:39 PM UTC

Hi 
I think so , here is my ioc file:

Thanks

mƎALLEm
ST Technical Moderator
Feb 14, 2025 6:50 PM UTC

Could you please replace the MPU config like the following?:

void MPU_Config(void)
{
 MPU_Region_InitTypeDef MPU_InitStruct = {0};

 /* Disables the MPU */
 HAL_MPU_Disable();

 /** Initializes and configures the Region and the memory to be protected
 */
 MPU_InitStruct.Enable = MPU_REGION_ENABLE;
 MPU_InitStruct.Number = MPU_REGION_NUMBER0;
 MPU_InitStruct.BaseAddress = 0x0;
 MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
 MPU_InitStruct.SubRegionDisable = 0x87;
 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
 MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

 HAL_MPU_ConfigRegion(&MPU_InitStruct);
 /* Enables the MPU */
 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 18, 2025 11:00 AM UTC

Hello,

I didn't find that exact device STM32H733VGT but tested your ioc file on NUCLEO-H723ZI board (STM32H723ZI) and I didn't reproduce the behavior.

Don't step into SCB_EnableICache() and SCB_EnableDCache().

If you put a break point on HAL_Init() and run, do you reach it? 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
amirshnAuthor
Associate III
Feb 18, 2025 2:21 PM UTC

Hi,

yeah, that's the case, unexpectedly if I put a breakpoint after these two (SCB_EnableICache() and SCB_EnableDCache()) , I'll reach HAL_Init(). (I just figured this out).

Could you tell me why is it behaving like this?

 

Thanks a lot for your help.