STM32H725RG Maximum ADC Clock Rate in 16-bit Mode
I was reading this application note which lists maximum clock rates for the ADC on the STM32H7 for the various packages at different resolutions
However, it appears to have been written before the release of the STM32H723/H725 product lines which feature the VFQFPN-68 package, and the aforementioned application note does not include clock rates for the package in question. The datasheet for the part does not list a maximum clock rate for the different resolutions, just a maximum silicon limited clock rate for the different voltage scaling levels. I have been unable to find an updated version of that application note.
I am considering the STM32H725RG for a motor control application, and would like to know what the maximum adc clock rate for that package is. I would guess that it would be between that of the BGA100 and LQFP100 packages, leaning towards the BGA since it has no leads.
Thank you.