Skip to main content
TKana.1
Associate III
Apr 15, 2026 1:16 PM UTC
Solved

STM32H725REV Max Core Clock

Hi,

 

Planning to use VFQFPN68 package. I am confused about the max core clock I can use. CubeMx shows 550MHz for every "Power Regulator Voltage Scale (0-3)".

I remember reading VFQFPN68 has only DCDC solution so max core clock is 400MHz

 

Can anyone explain please?

Thanks,

Tim

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 1:36 PM UTC

Hello,

I think you are talking about STM32H7 dual core that has that restriction in SMPS mode:

SMPS usage restriction from the DS.png

But STM32H723 doesn't have such restriction in SMPS mode:

mALLEm_0-1776260154680.png

See also FAQ: Why the DIRECT_SMPS_SUPPLY option is not shown in STM32CubeMX for STM32H7 MCUs

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

TDK
Apr 15, 2026 1:31 PM UTC

Max clock speed is 550 MHz.

TDK_0-1776259836377.png

Achieved only in VOS0 and BOOST.

TDK_1-1776259869516.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 1:36 PM UTC

Hello,

I think you are talking about STM32H7 dual core that has that restriction in SMPS mode:

SMPS usage restriction from the DS.png

But STM32H723 doesn't have such restriction in SMPS mode:

mALLEm_0-1776260154680.png

See also FAQ: Why the DIRECT_SMPS_SUPPLY option is not shown in STM32CubeMX for STM32H7 MCUs

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.