Skip to main content
JCase.1
Associate III
July 18, 2025
Question

STM32H725 TIM5 issue

I am using one of the 32 bit timers to measure intervals for fault protection on a HV pulse modulator.  I have an interrupt on EXTI that captures both leading and trailing edges of the command pulse.   In the service routine, I simply store the latest uptime and downtime to calc the pulsewidth and period....pretty simple.    The pulsewidth is pretty small, so I use the free-running SYSTICK (400 MHz) for pulsewidth, but it is only 24 bits, so I need to use a 32 bit timer for the pulse period, and do so at 50 MHz.

I initially coded this with TIM2, and it worked perfectly.  Then I realized that I needed to use TIM2 elsewhere because I already wired a different time-critical signal to the TIM2.ETR pin (the ETR interrupt latency is far less than the EXTI latency).  So I switched my code to use TIM5 for the period.   This did not work.   It bounces around semi-randomly, and by appearances is acting like a 16 bit timer.

I switched to TIM23, and again it works perfectly.  I searched this website, and found other entries complaining of TIM5 operation, one specifically saying it reverted to 16bit after a rollover.  I do not find any reference to this on the errata sheets.    I am fine with my TIM23 fix, so I don't have a problem, but if this is a hardware bug, it should be on the errata.

I am hard coding in assembly, no HAL, no CUBE.  My init code is the same for all three cases:

     set TIMx_PSC to 3      (prescale = 4 with 200 MHz base for 50 MHz ticks)

     set TIMx_ARR to 0xFFFFFFFF      (max reload, simply free run the timer)

     set TIMx_EGR to 1

     set TIMx_CNT to 0

     set TIMx_CR1 to 81

The appropriate RCC reset pin is strobed and the RCC enable pin is on, of course.

In the interrupt service, I am simply capturing TIMx_CNT and saving to SRAM for later inspection.

 

Is this a known feature, or am I doing something ***?

Thanks!

Jeff Casey

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
July 19, 2025

Read out and check/post actual content of TIM5 registers.

> In the interrupt service, I am simply capturing TIMx_CNT and saving to SRAM for later inspection.

How are you *capturing* TIM5_CNT exactly?

Do you mean *reading* by that?

JW