Skip to main content
Associate
August 9, 2023
Question

stm32h725 doesn't work.

  • August 9, 2023
  • 9 replies
  • 7950 views

sangmin_0-1691549389868.png

Hello, I looked at AN5419 and configured the stm32H725igk6 power supply circuit as shown in the following figure, but the external osc does not work and the st link is not connected to the MCU.

Is this product a model that must be configured using SMPS to operate?

This topic has been closed for replies.

9 replies

LCE
Principal II
August 9, 2023

SMPS is not a must, afaik.

More info, please...

So, you say you configured, so you have a custom board?

Please show the relevant schematics: power supply, crystal, ST-Link IO, Boot pin

And the relevant clock configuration code.

TDK
August 9, 2023

Also clarify "doesn't work" here. Can you connect via STM32CubeProgrammer (if not, what is error message)? Does it report a target voltage?

SMPS is optional.

If it's a custom board, most likely answer is a schematic or hardware issue.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Michal Dudka
Lead
August 9, 2023

Let me guess. You've generated project by CubeMX and forgot to properly set up power managment. Default CubeMX configuration uses SMPS. After power up, your MCU switch its power supply to SMPS,and lost power. Therefore you can't connect with St-link. That can be easily verified - just measure voltage at VCAP pins. If there isn't voltage between 1.0V to 1.3V... if not, simply connect external 1.2V source to that point, connect St-link and do chip erase.

sangminAuthor
Associate
August 12, 2023

OSCOSC

sangmin_2-1691818253672.png

Thanks for the various answers. Above is the circuit connected to the MCU.
STlink detects 3.2V voltage.
As a result of further confirmation, the circuit is configured using a 25MHz clock, but it is not oscillating.

Vcap voltage comes out as 1.0V..!

ST Technical Moderator
August 14, 2023

Hello @sangmin 

You can refer to STM32H735G-DK schematic as a reference. Sheet 4 out of 19 in MB1520C (st.com) explains the LDO mode in the following configuration:

  •  SB19, SB3, SB1: Fitted
  • SB20, SB2, SB18, SB16, SB21: Not Fitted 

Also refer to the datasheet for Vcap operating conditions.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
sangminAuthor
Associate
August 17, 2023

I set it up like the previous picture, but it doesn't work.
The smps are all connected to GND like the picture before I sent. Will this be a problem?

Visitor II
August 12, 2023

Additionally, could you provide more details about the nature of the "doesn't work" situation? Are you able to establish a connection using STM32CubeProgrammer? If not, could you share any error messages you're encountering? Does it display the target voltage information?

Please note that the use of SMPS is discretionary.

If your setup involves a custom board, the most probable explanation could be a schematic or hardware-related problem.

sangminAuthor
Associate
August 14, 2023

These pictures are the phenomena that appear when I try to connect the board through stlink.

What I did was change the setting value in the stlink utility.
I changed the access port / SWD frequency / Mode / Rest Mode.
All didn't work.

TDK
August 17, 2023

Use STM32CubeProgrammer, not the ST-Link Utility.

R130 looks like a potential problem. Inrush current will definitely make that voltage drop below the allowable.

The SMPS pins are fine if you're not using SMPS.

"If you feel a post has answered your question, please click ""Accept as Solution""."