Skip to main content
andrew_henseleit
Associate II
May 10, 2021
Question

STM32H723VET Lowest power mode questions using Cube IDE

  • May 10, 2021
  • 7 replies
  • 1845 views

I am using the Cube IDE to put the STM32H723VET into standby (which to my knowledge is the lowest power consumption). The code below is what I use, I just want to make sure this is doing things correctly and I haven't missed any settings or anything I haven't stopped. It does go to sleep and wake up but the current is higher than I think it should be. Trying to rule out something easy before I dig into Hardware!!

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); //clear WU flag

 HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4); //enable WU pin

 HAL_SuspendTick();

 HAL_PWR_EnterSTANDBYMode();

This topic has been closed for replies.

7 replies

Petr DAVID
ST Employee
May 11, 2021

Hello Andrew_henseleit,

I was checking your code relating to PWR_STANDBY_RTC example available in STM32H7Cube software package and it looks fine to me. What current consumption are you measuring? In the code example I have mentioned there is note about making sure not to miss any wake up event with recommended sequence:

  • Disable all used wakeup sources
  • Clear all related wakeup flags
  • Re-enable all used wakeup sources
  • Enter the Standby mode

But if you are using just now wake up source this probably not apply to you. Let me know about about the measurements you are getting.

andrew_henseleit
Associate II
May 17, 2021

I am measuring total system current. I now have a board with just a processor on it to isolate the issue. The lowest I can seem to get with 1 wakeup source (WAKEUP_PIN4_LOW) is 0.5mA. It does wake up but that seems too high still.

andrew_henseleit
Associate II
May 11, 2021

With our custom HW it runs nominal at 148mA but the sleep drops to 10mA. Its impossible for me to pull out just the power for the processor. I did notice AN5014 mentioned multi core needed for standby. I have updated the Standby in the HAL to match this statement and plan to test tomorrow.

Piranha
Principal III
May 15, 2021

Set DBGMCU_CR = 0; before entering standby mode and physically disconnect the debug probe.

andrew_henseleit
Associate II
May 17, 2021

The above line did not do anything to my sleep current. It appears that the issue lies somewhere in my system clock. If I sleep before that then everything is good. Clock settings attached, I do not use the RTC and have 2 external oscillators.

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Supply configuration update enable

 */

 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 /** Configure the main internal regulator output voltage

 */

 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters

 * in the RCC_OscInitTypeDef structure.

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLM = 3;

 RCC_OscInitStruct.PLL.PLLN = 68;

 RCC_OscInitStruct.PLL.PLLP = 1;

 RCC_OscInitStruct.PLL.PLLQ = 4;

 RCC_OscInitStruct.PLL.PLLR = 2;

 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;

 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;

 RCC_OscInitStruct.PLL.PLLFRACN = 6144;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

 /** Initializes the CPU, AHB and APB buses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

               |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2

               |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;

 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;

 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)

 {

  Error_Handler();

 }

}

andrew_henseleit
Associate II
May 17, 2021

Update #2. When I changed my wakeup pin polarity to LOW instead of HIGH, my micro goes into standby at 0.5mA. This still seems high to me, its supposed be a few microamps per the datasheet right?

 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); //clear WU flag

  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);

  HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_LOW); //enable WU pin

  HAL_SuspendTick();

  HAL_PWR_EnterSTANDBYMode();

andrew_henseleit
Associate II
May 18, 2021

Update #3. I have taken out all code, I have set the everything off, all I have connected is an external oscillator and the power supplies needed to turn the chip on. Still only goes to 110uA. I don't believe my supplies are taking up 108uA or Q current. This is literally the only code in the project. What could I still possibly be doing wrong here??

 HAL_Delay(5000);

 HAL_Delay(5000);

 HAL_Delay(5000);

 HAL_Delay(5000);

 HAL_Delay(5000);

 //GO TO SLEEP HERE

 //HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN4); //disable wakeup pin

 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); //clear WU flag

 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);

 //HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_LOW); //enable WU pin

 HAL_DisableDBGStandbyMode();

 HAL_DisableDomain3DBGStandbyMode();

 HAL_PWR_DisableBkUpAccess();

 HAL_PWR_DisablePVD();

 HAL_SuspendTick();

 HAL_PWR_EnterSTANDBYMode();