Skip to main content
FAndr.1
Associate
Jun 23, 2021 10:30 AM UTC
Solved

STM32H723VE dma don't work with adc

dma don't work with adc. After first writing dma set flag TEIF. Value wasn't written to buffer. I ported example (adc dma transfer) from stm32h743 to 723, it have this error too.

This topic has been closed for replies.

7 replies

Imen GH
ST Employee
Jun 23, 2021 11:04 AM UTC

Hello,

Welcome to STM32 Community!

Have you tried the STM32CubeH7 firmware example?

I recommend you that you run and get inspired from ADC_DMA example code in STM32CubeH7 at this path:

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Examples\ADC\ADC_DMA_Transfer

This example can help you. it describes how to configure and use the ADC to convert an external analog input and get the result using a DMA transfer through the HAL API.

Imen

FAndr.1
FAndr.1Author
Associate
Jun 24, 2021 2:15 AM UTC

Thank you, its was first what I had do. Only replace *.ld and change RCC PLL config for my mcu and crystal. The result is the same - dma stopped after conversion starting with TEIF. I add my test project. Its new clear project with only adc + dma.

TDK
Jun 24, 2021 2:22 AM UTC

Your variables are in DTCM which is not accessible to DMA.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
TDKBest answer
Jun 23, 2021 1:01 PM UTC
FAndr.1
FAndr.1Author
Associate
Jun 24, 2021 2:24 AM UTC

Thank you, I read this article and tried off D-cache but it had no effect. I will try replace buffet to D2 RAM later.