Associate
January 5, 2022
Solved
stm32H723 (nucleo) with SDMMC, FR_NOT_READY
- 1 reply
- 1429 views
I'm stock since a while now.
I use H723 nucleo board with a SD card socket, build for SPI, but I use it as SDMMC with 1bit wide.
this socket is ok with SD and SPI.
f_mount send FR_NOT_READY.
I have the same answer with or with out Sd card...
I use a logic analyser and I can see that the clock never stop after start
is anybody have a clue or a simple working project with H723 and SDMMC ?