Skip to main content
HMüll.4
Senior
September 8, 2025
Solved

STM32H723 large ADC offset

Hi,

I'm already aware of the application note from https://www.st.com/resource/en/application_note/an5354-getting-started-with-the-stm32h7-series-mcu-16bit-adc-stmicroelectronics.pdf but as it does not cover STM32H72*-MCUs, I have to afraid I need to ask it here.

I have configured some ADC-stuff for 16 bit data sampling in CubeMX but now get incredible large offsets, even when the ADC-pins are connected to GND directly. That offset is in range 2000..4000 and very instable, means floating about the full range (I except it not to be a noise-problem as for testign the pin is pulled to GND directly).

What I have configured in CubeMX:

VREFBUF-mode to internal voltage reference

Trimming Mode: factory trimming

Internal voltage reference scale: SCALE2 (around 1.8V as I expect input voltages in range 0..1,8V)

The ADC's are used without oversampling, asynchronous clock-mode, divided by 4. The clock to the ADC's is at 64 MHz (may be too high?)

ADC is running in independent mode, no continuous conversion and software-triggered start of conversion.

At the very beginning, prior to starting the ADCs, I call

HAL_ADCEx_Calibration_Start(&hadc1,ADC_CALIB_OFFSET_LINEARITY,ADC_SINGLE_ENDED);
HAL_ADCEx_Calibration_Start(&hadc1,ADC_CALIB_OFFSET,ADC_SINGLE_ENDED);

So...what could be missing? Anything to check to find the problems?

Thanks!

 

Edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code

This topic has been closed for replies.
TDK
TDKBest answer
September 8, 2025

Yes. Two capacitors, as outlined in the datasheet and elsewhere.

How to use VREFBUF peripheral on STM32 MCUs and MPUs - Application note

"If you feel a post has answered your question, please click ""Accept as Solution""."

10 replies

Ozone
Principal
September 8, 2025

I don't know details about the H7 specifically.

> The ADC's are used without oversampling, asynchronous clock-mode, divided by 4. The clock to the ADC's is at 64 MHz (may be too high?)

> ADC is running in independent mode, no continuous conversion and software-triggered start of conversion.

At the very beginning, prior to starting the ADCs, I call

What do you have connected to the ADC pins, and what sampling times you have configured ?
I would first try connecting them to GND, and expect around 0.

HMüll.4
HMüll.4Author
Senior
September 8, 2025


> I would first try connecting them to GND, and expect around 0.

This is what I'm doing and where i get these way too high offset-values...

> what sampling times you have configured ?

What do you mean exactly with "sampling time"?

 

Ozone
Principal
September 8, 2025

> What do you mean exactly with "sampling time"?

Check the reference manual and your (Cube/HAL) application code.


And:
Does you MCU has dedicated AGND pins ?
You need to connect the input to the ADC pin and AGND.
On most Nucleo/Discovery boards, AGND is connected to GND.

TDK
September 8, 2025

The symptoms suggest the pin is not pulled to ground. What board is this, and which pins?

"If you feel a post has answered your question, please click ""Accept as Solution""."
HMüll.4
HMüll.4Author
Senior
September 8, 2025

So what we have:

AGND is connected with general GND

VDDA is connected with general VDD (3.3V)

VREF+ is left open due to the internal reference configuration

The analogue inputs at PB0/PB1 (both configured as analog inputs with "no pull") come with a voltage divider to come from the 0..10V input value down to 0..1,8V range (with an op-amp in order to decouple this voltage divider from any inputs internal resistance):

ain.png

As you can see, it is a custom board, so no Nucleo or DK from ST.

 

TDK
September 8, 2025

> VREF+ is left open due to the internal reference configuration

Is VREF+ bypassed to GND with a 1 uF + 100 nF cap? Or just completely floating? It needs the caps to be stable.

TDK_0-1757335103787.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
HMüll.4
HMüll.4Author
Senior
September 8, 2025

> Is VREF+ bypassed to GND with a 1 uF + 100 nF cap? Or just completely floating? It needs the caps to be stable.

It is completely floating, right because VREG+ is configured in CubeMX  to be set internally completely. So this capacitor is still needed, even when I do not make use of this input?