Skip to main content
LCE
Principal III
Oct 23, 2026 4:19 PM UTC
Solved

STM32H723 .. 735 at 1.8V (because of HyperRam)

Heyho,

just when we got the quote from our PCB assembly company for a prototype of a big board with the STM32H733, I find that basically all HyperRam ICs with 3.3V are EOL. 

There’s no alternative to 8-pin HyperRam due to IOs, routing, and board space, so the best would be to switch the complete system from 3.3 V to 1.8 V.
BTW, I find that the HyperRams are working great with the H7, 11 IOs, only, fast, relatively low power, no problems at all so far.

It’s 2026, darn… I started working as an EE at around 2000, and then the 5V → 3.3V transition was mostly done. Now it’s time for 1.8 V.

Anyway, I checked the H73x datasheets, and looks like these are fully operable at 1.8V without any problems (only exception: the internal OPAMP needs >= 2.0V, but we don’t use that), at full clock and IO speed.

So my questions to the H723..H735 users:

  • Anything I did oversee or forgot ?
  • What’s your experience running the H7 at 1.8 V ?

Changing the rest of the components is another … PITA, but first I need to know if the H7 as the “heart and brains” of the system is fully capable at 1.8 V.

Please share your thoughts!

Thanks in advance!

STOne-32
STOne-32Best answer
ST Technical Moderator
Oct 29, 2026 4:27 PM UTC

Hi ​@LCE ,

yes this is possible on this MCU and all recent STM32 MCUs . If there is a limitation or constraints regarding power pins , it is clearly mentioned in the product datasheet . electrical AMR and operating  conditions .

Regards,

STOne-32

5 replies

STOne-32
ST Technical Moderator
Oct 24, 2026 1:30 PM UTC

Dear ​@LCE ,

 

1.8V is already de facto the standard for all STM32 consumers applications since the STM32F2 and STM32F4 series  and before H7 series and running at full speed and full potential such as I/O are boosted with HSLV mode to keep the same performance as it was with 3.3V and keeping the same robustness versus EMC stress , so matching the Robust Industrial Markets. further more  now , we introduced 1.2Volts I/O but with reduced performance.

The only care is for all analog / dynamic range such as ADC, DAC , OPAMP, and USB PHY , for that operations we have dedicated power supply pins at 3.3V and you can keep both rails on same PCB : all digital powers at 1.8V and specific Analog ( if required at application level ) with 3.3V.

Hope it helps ,

STOne-32 
 

LCE
LCEAuthor
Principal III
Oct 26, 2026 6:59 AM UTC

​@STOne-32  Thanks for the info!

I’m so used to the maximum rating VDDA <= VDD that I didn’t even check that…

Checking the H733 datasheet once more, I actually do not find that restriction,
so it is possible to have VDD = 1.8 V and VDDA = 3.3 V ?

 

Checking the L073 we’re using in a project related to that one, which also must use the 1.8 V as VDD, I find that the difference between VDDA and VDD must not be greater than 300 mV, correct ?

LCE
LCEAuthor
Principal III
Oct 26, 2026 2:18 PM UTC

> 1.8V is already de facto the standard for all STM32 consumers applications

industrial stuff here…

Anybody here using 1.8V as main VDD for STM32 in industrial environments?

Speaking of high power inverters close to our devices.

LCE
LCEAuthor
Principal III
Oct 29, 2026 8:25 AM UTC

​@STOne-32 could you please confirm this?

> so it is possible to have VDD = 1.8 V and VDDA = 3.3 V ?

 

So I would keep only VDDA at 3.3V, with an external VREF+ at 3.0V, all other VDD at 1.8V.

STOne-32
STOne-32Best answer
ST Technical Moderator
Oct 29, 2026 4:27 PM UTC

Hi ​@LCE ,

yes this is possible on this MCU and all recent STM32 MCUs . If there is a limitation or constraints regarding power pins , it is clearly mentioned in the product datasheet . electrical AMR and operating  conditions .

Regards,

STOne-32