Skip to main content
Associate III
February 25, 2026
Solved

STM32H7 with active D-Cache and sdMMC with DMA

I try to start working sdMMC with DMA. When D-Cache is not active work well. But when turn it on stop work. Probably need to create MPU region , but where is located used RAM from sdMMC. And if need, how to change .ld file?

 

DmitryR
DmitryRBest answer
Associate III
February 25, 2026

Hi @Brussl ,

 

RAM for sdMMC is the buffer you supply to subsequent functions. But using separate non-cacheable MPU region for their placement is not a good idea as it forces you to use static buffers at fixed address or dynamically reconfigure MPU. Both are not a good programming practices.

 

Actually buffers for reading and writing sdMMC may reside in any region reachable by the DMA of the sdMMC controller. When you read, just before using the buffer being read you should invalidate the cache for the memory region used by the buffer calling SCB_InvalidateDCache_by_Addr. When you write, you should call SCB_CleanDCache_by_Addr just before triggering the write.

 

With best regards,

Dmitry

7 replies

mƎALLEm
ST Technical Moderator
February 25, 2026

Hello,

You need to apply the cache maintenance when you enable the D-cache when using another master DMA/SDMMC/  CM4 (in dual core). You can disable the cache for the shared memory between the CM7 and the other master using the MPU (MPU policy: Device) but that decreases the performance.

Please refer to the application note AN4839 "Level 1 cache on STM32F7 Series and STM32H7 Series" / especially the section 3.2 Example for cache maintenance and data coherency.

screenshot.png

The different available solutions:

screenshot.png

Hope that answers your question.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
BrusslAuthor
Associate III
February 25, 2026

OK. And what is the region of RAM used by sdMMC ? The MCU is one core ,. just need to stop caching in this region. As I see sdMMC used MDMA. But where is allocated RAM? 

mƎALLEm
ST Technical Moderator
February 25, 2026

Please read the documentation especially the user manual of the product. From RM0433:

The memories accessible by SDMMC1 and SDMMC2:

screenshot.png

The RAM used by the SDMMC depends on the user configuration in his application.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
DmitryR
DmitryRBest answer
Associate III
February 25, 2026

Hi @Brussl ,

 

RAM for sdMMC is the buffer you supply to subsequent functions. But using separate non-cacheable MPU region for their placement is not a good idea as it forces you to use static buffers at fixed address or dynamically reconfigure MPU. Both are not a good programming practices.

 

Actually buffers for reading and writing sdMMC may reside in any region reachable by the DMA of the sdMMC controller. When you read, just before using the buffer being read you should invalidate the cache for the memory region used by the buffer calling SCB_InvalidateDCache_by_Addr. When you write, you should call SCB_CleanDCache_by_Addr just before triggering the write.

 

With best regards,

Dmitry

BrusslAuthor
Associate III
February 25, 2026

Ok DmitryR , and what is address and size that can invalidate ?

DmitryR
Associate III
February 25, 2026

Hi @Brussl ,

 

It is the address and size of the buffer that you supply to the subsequent HAL functions, HAL_SD_ReadBlocks and HAL_SD_WriteBlocks. If you use some file system then they are the buffers that you supply to the subsequent file system functions. 

 

Regards,

Dmitry