Skip to main content
ramkumarkoppu
Associate III
May 26, 2021
Question

STM32H7 vs STM32MP1 for heterogenous application use case

  • May 26, 2021
  • 1 reply
  • 1771 views

For one of the heterogenous application use case, we would like run always-on code in Cortex-M4 and high end application, we have two options. either run Cortex-M7 if se select STM32H7 device or Cortex-A7 if select STM32MP1 device. Assuming that both of these devices allow Cortex-M4 as always-on and high end CPU (either M7 for STM32H7 or A7 for STM32MP1) and ignoring Linux support, which device more energy efficient. is it STM32H7 or STM32MP1?

This topic has been closed for replies.

1 reply

Christophe Guibout
ST Employee
June 16, 2021

Hi @ramkumarkoppu​ ,

The article How to define your low-power strategy in STM32MP1 wiki gives some power figures.

Hope it will help.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.