Question
STM32H7 SPI IRQn never triggered
Hi,
I am using SPI1 and interrupt are enabled in this function
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
........................
/* SPI1 interrupt Init */
HAL_NVIC_SetPriority(SPI1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}Spi works fine in blocking mode, I want to switch to DMA mode but I never enter this function :
void SPI1_IRQHandler(void)
{
/* USER CODE BEGIN SPI1_IRQn 0 */
/* USER CODE END SPI1_IRQn 0 */
HAL_SPI_IRQHandler(&hspi1);
/* USER CODE BEGIN SPI1_IRQn 1 */
/* USER CODE END SPI1_IRQn 1 */
}Any ideas why my interrupts are never triggered ?
Gabriel