STM32H7 SPI_FullDuplex_ComDMA example
Hi,
In the SPI_FullDuplex_ComDMA example from STM32Cube_FW_H7_V1.2.0, if the aTxBuffer is changed from const uint8_t to uint8_t. (from flash to sram). The code below:
for(i=0;i<128;i++) aTxBuffer[i] = 0x55;
SCB_CleanDCache_by_Addr((uint32_t *) aTxBuffer, 128);
HAL_SPI_TransmitReceive_DMA(&SpiHandle,(uint8_t*) aTxBuffer, (uint8_t *) aRxBuffer, 128);
The Data in MOSI pin is 0x55 only if the SCB_CleanDCache_by_Addr is called, otherwise MOSI pin show no data, always zero.
I would like to know why this is necessary for the H7 and not for F7?
And how can I configure the MPU so that the
SCB_CleanDCache_by_Addr
call is not required?Ari.