Skip to main content
MPete.3
Associate II
July 5, 2022
Question

STM32H7 Segger J-Link Debugging Issue

  • July 5, 2022
  • 6 replies
  • 4938 views

Hello,

When trying to do a debug session onto these different STM32H7 devices:

  • STM32H743IIT6 / STM32H753IIT6
  • STM32H7A3IGT6

we are receiving the error

0693W00000QKUdHQAX.pngwith the following console statements:

SEGGER J-Link GDB Server V7.62a Command Line Version
 
JLinkARM.dll V7.62a (DLL compiled Feb 23 2022 16:58:13)
 
Command line: -port 2331 -s -device STM32H753II -endian little -speed 12000 -if swd -vd
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: off
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: STM32H753II
Target interface: SWD
Target interface speed: 12000kHz
Target endian: little
 
Connecting to J-Link...
J-Link is connected.
Firmware: J-Link V10 compiled Nov 2 2021 12:14:50
Hardware: V10.10
S/N: 50100143
Feature(s): GDB
Checking target voltage...
Target voltage: 3.31 V
Listening on TCP/IP port 2331
Connecting to target...
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x08049122 (Data = 0x4B09681A)
Received monitor command: WriteDP 0x2 0xF0
O.K.
Read 4 bytes @ address 0x24066F48 (Data = 0x00000001)
Read 4 bytes @ address 0x24066A68 (Data = 0x24065DE0)
Reading 32 bytes @ address 0x24066ECC
Reading 32 bytes @ address 0x240116B8
Reading 516 bytes @ address 0x240116B4
Reading 32 bytes @ address 0x24029A18
Reading 516 bytes @ address 0x24029A14
Reading 32 bytes @ address 0x240660B0
Reading 516 bytes @ address 0x240660AC
Reading 32 bytes @ address 0x240207A8
Reading 516 bytes @ address 0x240207A4
Reading 32 bytes @ address 0x2400A448
Reading 516 bytes @ address 0x2400A444
Reading 32 bytes @ address 0x24024878
Reading 516 bytes @ address 0x24024874
Reading 32 bytes @ address 0x24066EE0
Reading 32 bytes @ address 0x240072A8
Reading 516 bytes @ address 0x240072A4
Reading 32 bytes @ address 0x240169F8
Reading 516 bytes @ address 0x240169F4
Reading 32 bytes @ address 0x24018398
Reading 516 bytes @ address 0x24018394
Reading 32 bytes @ address 0x24017AC8
Reading 516 bytes @ address 0x24017AC4
Reading 32 bytes @ address 0x24016128
Reading 516 bytes @ address 0x24016124
Reading 32 bytes @ address 0x24066EFC
Reading 32 bytes @ address 0x24066F28
Reading 32 bytes @ address 0x24014058
Reading 516 bytes @ address 0x24014054
Reading 32 bytes @ address 0x24019468
Reading 516 bytes @ address 0x24019464
Reading 32 bytes @ address 0x24019D38
Reading 516 bytes @ address 0x24019D34
Reading 32 bytes @ address 0x2401E6D8
Reading 516 bytes @ address 0x2401E6D4
Reading 32 bytes @ address 0x2401A608
Reading 516 bytes @ address 0x2401A604
Reading 32 bytes @ address 0x2400B518
Reading 516 bytes @ address 0x2400B514
Reading 32 bytes @ address 0x24028948
Reading 516 bytes @ address 0x24028944
Reading 32 bytes @ address 0x24009378
Reading 516 bytes @ address 0x24009374
Reading 32 bytes @ address 0x2400F5E8
Reading 516 bytes @ address 0x2400F5E4
Reading 32 bytes @ address 0x24013788
Reading 516 bytes @ address 0x24013784
Read 4 bytes @ address 0x24066F44 (Data = 0x00000000)
Reading 32 bytes @ address 0x24066A6C
Reading 32 bytes @ address 0x24065DE4
Reading 516 bytes @ address 0x24065DE0
Received monitor command: ReadAP 0x2
O.K.:0x00000000
Reading 32 bytes @ address 0xE00FFFD0
Reading 32 bytes @ address 0xF0000FD0
WARNING: Failed to read memory @ address 0xF0000FD0
WARNING: Failed to read memory @ address 0xF0000FD0
WARNING: Failed to read memory @ address 0xF0000FEF
GDB closed TCP/IP connection (Socket 1084)
Restoring target state and closing J-Link connection...
Shutting down...

We are able to connect most of the time, but there are times when we have to re-start the debugger 5+ times of getting this error before it will finally attach. We have tried a Segger J-Link Base / Plus / Pro and all exhibit the same issue. We have also tried different programming speeds (console captured w/ 12000khz)

Is this an issue on Segger's side, or is this an issue with STM32CubeIDE trying to verify the ID of the STM?

Extra info:

0693W00000QKUdqQAH.png 

Thanks,

Marshall

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
July 6, 2022

Is the device on a devboard, or a custom board?

If custom board, is it a new design, or something well tested and known-working?

Have you ever had this working before?

Have you checked the wiring carefully - including things like grounds?

Does the Target Sleep, and/or disable the debug access pins?

Have you tried with, say, an ST-Link?

Have you tried a different debugger/programmer; eg, Segger's own tools?

Segger have a page on diagnosing J-Link connection issues:

https://wiki.segger.com/J-Link_cannot_connect_to_the_CPU

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MPete.3
MPete.3Author
Associate II
July 6, 2022

Is the device on a devboard, or a custom board?

Custom Board

 

If custom board, is it a new design, or something well tested and known-working?

Have you ever had this working before?

New Design, however this same exact layout works on many of our other STM32-based products. I also mentioned in the opening thread that it does connect, and i am able to debug / step / breakpoint / live expression / reset / etc. without issue, once it gets past the issue of "Verify ST device".

Have you checked the wiring carefully - including things like grounds?

Yes. We are using a Tag-Connect (and not our first product that does, and same header works on all of our other products) 

Does the Target Sleep, and/or disable the debug access pins?

Yes, the target can go to sleep (Standby with D2 and D3 shutoff / RTC On) for the STM32H743 / STM32H753, but the STM32H7A3 unit does not go to sleep... and both exhibit the same issue.

Have you tried with, say, an ST-Link?

Yes, i have just tried it with an ST-Link V3 and it has not experienced the same issue. I was able to Terminate and Relaunch 10x with no issue. 

Have you tried a different debugger/programmer; eg, Segger's own tools?

Yes, and it connects just fine every time using Segger J-Link Flash / GDB Server... however, if used in conjunction with STM32CubeIDE, the IDE cannot always connect (Sometimes it will, sometimes not)

Pavel A.
July 6, 2022

> it connects just fine every time using Segger J-Link Flash / GDB Server... however, if used in conjunction with STM32CubeIDE

IIRC this issue was already mentioned here. CubeIDE does not work well with some J-LINKs or some firmware versions, or only with certain MCUs ?