STM32H7 Power down sequence
About Power-Down Sequence (Device : STM32H7B0xB)
Datasheet : DS13196 - Rev 6 Page 13
"During the power-down phase, VDD can temporarily become lower than other supplies only if the energy provided to the microcontroller remains below 1 mJ. "
Could you please let me know what this description means?
The basic requirements for power sequence are as follows,
"When VDD is below 1 V, other power supplies (VDDA, VDD33USB and VDD50USB) must remain below VDD +300 mV."
I want to know the relationship between this basic requirement and "below 1mJ".
Is it an exception to the basic requirements?