Question
STM32H7 PLLFRACN Support
Posted on April 19, 2018 at 21:26
Are there plans to fully support the STM32H7 PLL fractional multiplier (PLLFRACN) for all 3 PLLs in STM32CubeMX? The RCC Configuration allows the PLL1 fractional value to be set, but not for PLL2 and PLL3. Setting the PLL1 fractional value is not reflected in the Clock Configuration tab. It would be great if the fractional value for each PLL could be entered in the Clock Configuration tab and that value automatically entered in the Configuration tab. Actually any additional STM32CubeMX support for PLLFRACN would be welcomed.
#pll-fractional-multiplier