Skip to main content
Associate
April 15, 2025
Question

STM32H7 MDMA With QSPI

  • April 15, 2025
  • 1 reply
  • 795 views

Hi,

 

I would like to use the MDMA with the QSPI on an STM32H743 or similar.

I need to use the QSPI to interface with several multiplexed LCD displays and I want to use the QSPI in 'indirect' mode to send commands to the displays and DMA the pixel data into the QSPI to transfer to the display.

I am a bit confused about how the MDMA is supposed to work - the reference manual says that QSPI can trigger the MDMA when the QSPI data FIFO reaches a threshold.

So I think I would use MDMA in 'buffer' transfer with TRGM = 00 - so each trigger from the QSPI transfers a buffers worth of data (to fill the QPSI FIFO), then configure the MDMA channel to run in 'block repeat' mode to transfer a whole frame buffer's worth of data (about 285 kB)

Am I thinking along the right lines here? The documentation for the MDMA seems pretty terse I don't know if I've understood it correctly.

But most importantly, how do I actually set an MDMA channel to take its trigger from QSPI? There is the field TSEL in the MDMA_CxTBR register, but I can't find any documentation anywhere that explains what hardware triggers are mapped by what values of TSEL... Or am I completely misunderstanding how this works?

 

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
April 15, 2025

Hello @JF999 and welcome to the community,

 

Each MDMA channel provides an unidirectional transfer link between a source and a destination.
Each channel can perform transfer of the following types:
• Single block transfer: one block is transferred. At the end of the block, the MDMA channel is disabled and an end-of-channel transfer interrupt is generated.
• Repeated block transfer: a number of blocks is transferred before disabling the channel.
• Linked-list transfer: when the transfer of the current data block (or last block in a repeat) is completed, a new block control structure is loaded from memory and a new block transfer is started.

For more information about different mode transfer, I recommend you to look at RM0433 precisely 14. MDMA controller (MDMA).

For the QUADSPI transfer with MDMA, I think the AN4760 section DMA usage and QSPI_ReadWrite_DMA example can help you.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.