Skip to main content
Visitor II
Nov 12, 2025 5:51 AM UTC
Solved

stm32H7 LTDC confusion

Hello, I want to use LTDC on the STM32H743VIT6 microcontroller, but when I enable this peripheral in CUBEMX, it does not activate correctly. For example, the pins for B are from B3-B7, while they should be from B0-B4, and the same goes for R, G.

HOSI_0-1762926289188.png

 

Issamos
IssamosBest answer
Super User
Nov 12, 2025 8:10 AM UTC

Hello @HOSI 

I’m not an LTDC expert. But, think this is normal and no problem with this configuration according to the figure 32 of the AN4861, on a RGB666 display, the B  pins should be from B2 to B7 and not from B0 to B5 as on the display side. Same for G and R pins:

Issamos_0-1762934863382.png

Best Regards.

II

1 reply

Issamos
IssamosBest answer
Super User
Nov 12, 2025 8:10 AM UTC

Hello @HOSI 

I’m not an LTDC expert. But, think this is normal and no problem with this configuration according to the figure 32 of the AN4861, on a RGB666 display, the B  pins should be from B2 to B7 and not from B0 to B5 as on the display side. Same for G and R pins:

Issamos_0-1762934863382.png

Best Regards.

II