Question
STM32H7 -FMC - LCD INTEFACE - A19 AS REGISTER SELECT
Hi,
When A0 is used as Register select in the FMC LCD interface, ST uses the code below:
typedef struct
{
__IO uint16_t REG;
__IO uint16_t RAM;
}LCD_CONTROLLER_TypeDef;
/* We use BANK1 as we use FMC_NE1 signal */
#define FMC_BANK1_BASE ((uint32_t)(0x60000000 | 0x00000000))
#define FMC_BANK1 ((LCD_CONTROLLER_TypeDef *) FMC_BANK1_BASE)
FMC_BANK1->RAM = Data; //Write Data
FMC_BANK1->REG = cmd; ///write CMD
How to do it when the Register select is A19?