Skip to main content
Associate II
May 7, 2024 2:41 AM UTC
Question

STM32H7 支持的协议

STM32H7 can support SPI communication, Parallel communication, GPIO analog SPI communication, but can it support TTL, SDR CMOS, JESD204B protocol communication? Or what should I do if I want STM32 to implement these protocols?

This topic has been closed for replies.

2 replies

mƎALLEm
ST Technical Moderator
May 7, 2024 4:36 PM UTC

Hello,

STM32 does not implement JESD204B standard. GPIO emulation is the only solution available which is not an easy task taking into account timing constraints etc ..

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
May 7, 2024 10:03 PM UTC

>>Or what should I do if I want STM32 to implement these protocols?

Bolt on an FPGA / CPLD ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..