Question
STM32H573 SDMMC NEGEDGE valid/hold time
Dear ST Community,
I am using the STM32H573's SDMMC interface to communicate with a soft eMMC device implemented in FPGA:
- 1.8V I/O
- DDR==0 mode
- CLKDIV>0.
I'm setting up the timing constraints for the FPGA's CMD input versus the CK input and I have a query about the SDMMC interface timing.
In the datasheet, Table 123 defines the tov and toh parameters. In which mode are these parameters valid? CLKDIV>0 and NEGEDGE==0?
How would NEGEDGE==1 change tov and toh? Based on the diagrams of figure 164, I believe the tov and toh would increase by 1/2 the clock period. Is that correct?
Thank you. Ben