Skip to main content
Associate
Oct 15, 2026 4:26 AM UTC
Question

STM32H563VIT3Q Controller Communication Failure During ISO 16750-2:2023 Superimposed Alternating Voltage Test

Hi Team,

 

We are performing the ISO 16750-2:2023 Superimposed Alternating Voltage test on our DUT. The 12 V main supply is provided to the TPSM64406RCHR buck converter, which generates a nominal 3.3 V supply for the STM32H563VIT3Q controller.

During the test, a 6 V peak-to-peak AC ripple is superimposed on the 12 V input, causing the input voltage to vary between approximately 9 V and 15 V. Under this condition, communication with the STM32 controller fails.

We attempted to reflash the firmware multiple times, but the issue persisted. However, when we performed a Full Chip Erase using STM32CubeProgrammer and then reflashed the firmware, the controller started working properly.

Could you help us identify the possible root cause of this issue and explain why repeated firmware flashing did not resolve it, whereas a full chip erase followed by reflashing restored normal operation? We would also appreciate recommendations for further debugging to determine whether the issue is related to power supply instability, MCU reset or boot behavior, Flash memory contents, or firmware execution during the superimposed alternating voltage test.

 

 

Thanks,

Ramesh 

2 replies

Ramesh_pbAuthor
Associate
Oct 19, 2026 4:39 AM UTC

Hi Team,

Could you please clarify the query at the earliest?

Thanks & Regards,
Ramesh

ST Technical Moderator
Nov 5, 2026 4:47 PM UTC

Hi ​@Ramesh_pb 

To help narrow this down, could you share the test frequency and oscilloscope captures of the 12 V input, the MCU’s 3.3 V supply, and NRST during the test. Can you clarify whether the MCU resets when communication is lost or continues running?

If the issue occurs again, save the Flash contents and device configuration before erasing the MCU

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL