Skip to main content
Associate
August 5, 2024
Question

STM32H563 Custom External Loader Issues

I am trying to build a custom external loader for W25Q64 SPI. I am using the OCTOSPI1 using the follow pins.

PE11OCTOSPI1_NCS
PF6OCTOSPI1_IO3
PF7OCTOSPI1_IO2
PF8OCTOSPI1_IO0
PF9OCTOSPI1_IO1
PF10OCTOSPI1_CLK

I have followed the stm32-external-loader/Demo_Project as template. Currently I have no issue when making a example project using external loader function calls. I can read/write/erase without issue.

However, when the .stdr is used in STM32CubeProgrammer v2.17.0 GUI and command line it fails to do anything.

I get the following:

Reading data...
halt ap 1
w ap 1 reg 15 PC (0x20003000)
w ap 1 reg 17 MSP (0x20003500)
w ap 1 reg 16 xPSR (0x01000000)
Init flashloader...
halt ap 1
w ap 1 reg 0 R0 0x00000000
w ap 1 reg 1 R1 0x00000000
w ap 1 reg 2 R2 0x00000000
w ap 1 reg 3 R3 0x00000000
w ap 1 reg 4 R4 0x00000000
w ap 1 reg 5 R5 0x00000000
w ap 1 reg 6 R6 0x00000000
w ap 1 reg 7 R7 0x00000000
w ap 1 reg 8 R8 0x00000000
w ap 1 reg 9 R9 0x00000000
w ap 1 reg 10 R10 0x00000000
w ap 1 reg 11 R11 0x00000000
w ap 1 reg 12 R12 0x00000000
w ap 1 reg 13 SP 0x00000000
w ap 1 reg 14 LR 0x00000000
w ap 1 reg 15 PC 0x20003521
w ap 1 reg 16 xPSR 0x01000000
w ap 1 reg 17 MSP 0x00000000
w ap 1 reg 18 PSP 0x00000000
run ap 1
halt ap 1
r ap 1 reg 0 R0 0x00000000
Init function fail
r ap 1 reg 16 xPSR 0x01000003
halt ap 1
w ap 1 reg 15 PC (0x20003000)
w ap 1 reg 17 MSP (0x20003500)
w ap 1 reg 16 xPSR (0x01000000)
Error: failed to read the requested memory content

I believe this issue is something with LR and MSP registers not being assigned. However, I am not sure how to go about doing that. I have tried to added debug with LEDs, however it never enters the Init function. The PC appears to point to the Init function

Note: I only have access to STM32CubeIDE.

 

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
August 5, 2024

It's claiming it called Init() and you returned zero (fail code)

There's no static initialization occurring, so no startup.s, SystemInit() or main() being called. There shouldn't be a vector table, and you shouldn't be using interrupts.

You can perhaps use a UART to communicate, or a GPIO / LED in some form or fashion

The build basis for RAM should be 0x20003004, and not 0x20000004 (most) or 0x24000004 (H7)

RAM_PROG (xrw) : ORIGIN = 0x20003004, LENGTH = 256K-12292

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
August 6, 2024
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
lkantoskiAuthor
Associate
August 6, 2024

Thank you for the support. 

 

I believe I found my issue.

After many build attempts, I determined there was a linker issues. I simplified my function calls to just return 1, CubeProgrammer still failed and list that my LR and MSP were both 0x00000000.

In my failing state I turned off "Discard unused sections" in the linker, to preserve my function calls. This appears to be what was causing my issue.

The solutions was:

Leave "Discard unused sections" enabled

In the linker script, add the following to the .text section

 

 

 

KEEP (*(.text.Init))
KEEP (*(.text.DeInit))
KEEP (*(.text.Write))
KEEP (*(.text.Read))
KEEP (*(.text.Verify))
KEEP (*(.text.Checksum))
KEEP (*(.text.SectorErase))
KEEP (*(.text.MassErase))

 

 

After building this way, my Init was no longer failing out and the LR and MSP were both real values.

Now I need to revert my code to make actual calls.

 

 

Tesla DeLorean
Guru
August 6, 2024

Yes, that's what I did with my example using GNU/GCC + MAKE in a free standing way.

https://github.com/cturvey/stm32extldr/blob/main/ExternalLoader_H5.ld

Might look at objdump to see what's kept, exported, or discarded.

@STTwo-32 can someone check if STM32 Cube Programmer reports issues/errors if the External Loader doesn't export Init or StorageInfo ? And perhaps explain or document the H5 use of the 0x20003004 RAM basis

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..