Skip to main content
Associate
Jun 4, 2025 8:32 AM UTC
Solved

STM32H562 Ethernet Erratum 2.22.10

According to erratum 2.22.10 of STM32H562xx/563xx/573xx in RMII 10MHz mode packets should be accepted when both dribble and CRC error is flagged.

 

According to Reference Manual RM0481 Rev4 Table 692 dribble bit is valid in MII mode only.

 

Pls. clarify 

 

 

This topic has been closed for replies.
STackPointer64Best answer
ST Employee
Jun 4, 2025 11:16 AM UTC

Hello @Nabidev,

First, I would like to welcome you to the community.

Second, the point you just mentioned occurs when working with RMII at 10 MHz. As explained in erratum 2.22.10, dribble errors are rare, but when they happen, the extra nibble caused by the PHY results in a CRC error, which leads to the received packet being dropped.

That is why you should consider the Dribble bit error only when working in MII mode. Encountering such an error with RMII at 10 MHz causes packet drops due to the CRC error bit being flagged. The solution is to enable error packet forwarding (FEP) to resolve it.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.

1 reply

STackPointer64Best answer
ST Employee
Jun 4, 2025 11:16 AM UTC

Hello @Nabidev,

First, I would like to welcome you to the community.

Second, the point you just mentioned occurs when working with RMII at 10 MHz. As explained in erratum 2.22.10, dribble errors are rare, but when they happen, the extra nibble caused by the PHY results in a CRC error, which leads to the received packet being dropped.

That is why you should consider the Dribble bit error only when working in MII mode. Encountering such an error with RMII at 10 MHz causes packet drops due to the CRC error bit being flagged. The solution is to enable error packet forwarding (FEP) to resolve it.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.