Skip to main content
MKout.1
Visitor II
April 6, 2023
Question

STM32H562 - application note/out of box example for SAI with PDM mic

  • April 6, 2023
  • 1 reply
  • 894 views

At the moment, we evaluate feasibility of STM32H562 for our application. Our application is using PDM microphones. However, STM32H562 has SAI interfaces but no DFSDM filters.

Is there any out of box application example /application note for PDM microphone with SAI interface? (multichannel solution for 4 PDMs would be nice, 2 PDMs is a must)

This topic has been closed for replies.

1 reply

ST Technical Moderator
April 6, 2023

Hello @MKout.1​ and welcome to the Community :)

Currently, there is no available SAI application for STM32H5.

Maybe you can review and get inspired from the SAI application with STM32CubeU5 MCU package:

\STM32Cube_FW_U5_Vx.x.x\Projects\STM32U575I-EV\Examples\SAI\SAI_AudioPlay

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks