Skip to main content
Associate III
January 17, 2025
Question

STM32H533 DCACHE seems to make no difference?

So I've got a program with a fast tight loop doing some minimal things, and the rest is housekeeping/UI stuff in the main loop. When I enabled ICACHE, the speed of the tight loop increased DRAMATICALLY and overall the process is faster at basically everything. A colleague of mine said that he uses the DCACHE also and that for his application on an H7, the DCACHE made a huge performance improvement. But, as far as I can measure (which is toggling GPIO pins at critical sections of code and measuring the time with o-scope), the DCACHE made no difference on or off.

 

So for now I 'm just leaving it off because I know I need to be careful with DCACHE and my SD Card etc. and it's easier to just leave it off, but I'm wondering what areas/use cases is the DCACHE actually supposed to improve with this chip?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
January 17, 2025

Per the Reference Manual the connectivity for the DCACHE (4KB) is the OCTOSPI and FMC, so code/data on external memories likely to be where you'd see it.

The SRAMs all look to be relatively closely coupled

https://www.st.com/resource/en/reference_manual/rm0481-stm32h52333xx-stm32h56263xx-and-stm32h573xx-armbased-32bit-mcus-stmicroelectronics.pdf#page=107

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
devinwAuthor
Associate III
January 17, 2025

Thanks, that's a good point. I'm not using the OCTOSPI or the FMC for anything, so that would correlate to what I'm seeing.

Tesla DeLorean
Guru
January 17, 2025

Not sure the caching would impact the SDMMC in this context.

The H7 is a particularly odd beast, designed as a dual core, with dual ported memories. The F7 on the other hand can use the DTCM for SDMMC DMA, and that's not cached.

You want the DMA 4-byte aligned. On the H7 the cache lines are 32-byte aligned, and SDMMC there is workable with care, as the clear/invalidate by address need to span the buffer, it they are miss-aligned you can get collateral damage to structures directly abutting the SDMMC DMA buffer.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..