Skip to main content
Associate III
Oct 9, 2024 11:14 AM UTC
Solved

STM32H523CE RTC wakeup

I want to use the on-board RTC while all power (except VBAT which will be connected to a battery) is turned off to retain the clock.

Is it possible to power the on-board RTC from VBAT and turn off ALL other supplies?

What will happen after the other supplies are turned on again together with a POR?

Can one of the VBAT GPIOs be used to signal an RTC event with only VBAT powered (want to use this to wakeup)?

This topic has been closed for replies.
PGump.1
PGump.1Best answer
Senior II
Oct 9, 2024 12:26 PM UTC

Hi,

Yes you can. Use the RTC_OUT pin to control VCC.

Kind regards
Pedro

 

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.

5 replies

waclawek.jan
Super User
Oct 9, 2024 12:23 PM UTC

> Is it possible to power the on-board RTC from VBAT and turn off ALL other supplies?

Yes. That's the purpose of VBAT.

> What will happen after the other supplies are turned on again together with a POR?

What would you expect to "happen"?

> Can one of the VBAT GPIOs be used to signal an RTC event with only VBAT powered (want to use this to wakeup)?

I don't know what do you mean by "RTC event", but reading the Power, RTC and TAMP chapters in RM will answer your question.

JW

 

thansenAuthor
Associate III
Oct 9, 2024 1:48 PM UTC

I want to wake up at a specific time.

PGump.1
PGump.1Best answer
Senior II
Oct 9, 2024 12:26 PM UTC

Hi,

Yes you can. Use the RTC_OUT pin to control VCC.

Kind regards
Pedro

 

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
thansenAuthor
Associate III
Oct 9, 2024 1:49 PM UTC

Thank you Pedro I think that answers my question.