Skip to main content
Associate
November 25, 2024
Question

stm32h503 how read multi channel value in interrupt mode

Hello evryone:

at the first it is may firt project with STM32, and don't have any experince with this MCU.

I have a problem, when I read (with HAL_ADC_GetValue(&hadc1)) the multi channel ADC value in interrupt mode the value is always the same. I have tryed all type setup in STM32CUBE IDE, but the result is always same.

There evryone to help me?

Tanks and sorry for my poor english.

This topic has been closed for replies.

4 replies

gbm
Super User
November 25, 2024

1. Use DMA for multiple channels - classic STM32 technique.

2. It's generally not a good idea to use ADC interrupts.

3. To handle multiple channels without DMA you may use AUTDLY setting in ADC config register,

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Giomer59Author
Associate
November 25, 2024

I would like to use DMA memory, but the setup in GPDM1 or 2 is not very easy for me (much easier with STM32F302). I would like to have an example of how to do it. Also, the suggestion to use AUTDLY is unfamiliar to me. Could you point me to where I can find something that might help me?

ST Employee
November 26, 2024
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.