Skip to main content
Terry Greeniaus
Senior
May 22, 2026 1:11 AM UTC
Solved

STM32H503 ADC1 DS14053 Rev 4 vs. RM0492 Rev 3

There seems to be a documentation error between DS14053 Rev 4 and RM0492 Rev 3.  In the data sheet, section 3.17, table 3, "ADC Features" we see a different set of features compared to the reference manual, section 19.3, table 107.  The data sheet claims oversampling up to x1024, a data register of 32 bits and gain compensation is supported.  The reference manual claims oversampling up to x256, a data register of 16 bits and no gain compensation.

The register set description only has oversampling fields with values up to 256.  It would be helpful if ST could correct whichever document is wrong, and if the reference manual is wrong and oversampling up to x1024 is supported, then please also correct the register definitions.

Thanks,

TG

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 21, 2026 1:31 PM UTC

Hello,

The reference manual is correct i.e. table 107 in section 19.3 of RM0492 rev3. The datasheet will be updated.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
ST Technical Moderator
May 22, 2026 7:34 AM UTC

Hello @Terry Greeniaus ,

I will escalate the case internally for analysis and for eventual fix.

Internal ticket for follow-up: CDM0062840

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jul 21, 2026 1:31 PM UTC

Hello,

The reference manual is correct i.e. table 107 in section 19.3 of RM0492 rev3. The datasheet will be updated.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.