Skip to main content
CTabo.1
Senior
Feb 15, 2024 10:25 AM UTC
Question

STM32H5 USART RXFIFO error handing

Hello,
I am developing a serial communication driver using USART.
I have enabled FIFO and RTO interrupt, to handle reception.

TRM says that the received data is stored in the RXFIFO together with the corresponding flags and that PE, FE, NE bits in ISR register are associated with the character in the RDR register.

I would like to know which is the correct way to handle rx error.

In particular, when the RTO event occours (reception done), for each character present in the RXFIFO, should I first read the RDR register and then check the error flags in the ISR register, or viceversa?

Regards,
Carlo

 

This topic has been closed for replies.

5 replies

Karl Yamashita
Principal
Feb 16, 2024 1:44 AM UTC

The HAL driver automatically handles the error and clears the flag. It saves the error(s) in huart->ErrorCode and calls HAL_UART_ErrorCallback

In the callback, It's up to you to then check the error bits and act upon it accordingly.  

/** @defgroup UART_Error_Definition UART Error Definition
 * @{
 */
#define HAL_UART_ERROR_NONE (0x00000000U) /*!< No error */
#define HAL_UART_ERROR_PE (0x00000001U) /*!< Parity error */
#define HAL_UART_ERROR_NE (0x00000002U) /*!< Noise error */
#define HAL_UART_ERROR_FE (0x00000004U) /*!< Frame error */
#define HAL_UART_ERROR_ORE (0x00000008U) /*!< Overrun error */
#define HAL_UART_ERROR_DMA (0x00000010U) /*!< DMA transfer error */
#define HAL_UART_ERROR_RTO (0x00000020U) /*!< Receiver Timeout error */

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Lead II
Feb 16, 2024 4:59 AM UTC

Yes, the HAL Drivers should handle already errors (at least to clear them).

Why do you get a RFIFO Error?
Is your FW too slow? Do you miss an INT?

I would solve this RXFIFO error (instead to ask how to handle it: you would have lost data anyway).

CTabo.1
CTabo.1Author
Senior
Feb 19, 2024 12:58 PM UTC

Hello @Karl Yamashita and @tjaekel,
for performance reasons I am using LL rather than HAL driver.

Anyway, despite the way used to access USART registers, I am interested in the correct sequence for handling USART reception.

Should I first read the character from RDR register and the check the presence of the associated pending error flags, or should I first check the presence of error flags associated with the character in the RDR register and then read it?

I am not having FIFO errors, but I simply want to check if the received caracters are affected by errors (PE, FE, NE).

 

Regards,
Carlo

 

Karl Yamashita
Principal
Feb 19, 2024 3:44 PM UTC

See the sequence the HAL driver is doing. Use or don't use what you think is important to use.  

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
CTabo.1
CTabo.1Author
Senior
Feb 26, 2024 11:16 AM UTC

Hello,

from a brief analisys of HAL_UART_IRQHandler() function, it seems that the right sequence is first check the presence of error flags associated with the character in the RDR register and then read it.

Regards,
Carlo