Skip to main content
Associate II
Apr 13, 2026 5:38 PM UTC
Solved

STM32H5 JTDO/TRACESWO pin not working as UART7_RX despite alternate function support

Hi ST community,

I’m working with an STM32H563 MCU and trying to use the pin labeled JTDO/TRACESWO as UART7_RX because the datasheet/alternate function table shows that this pin supports UART7_RX.

 

However, UART transmission works correctly, but UART reception does not work when using this pin. If I switch to a different pin, both TX and RX function as expected.

Here’s what I’ve checked so far:

  • Configured the pin in STM32CubeMX as UART7_RX (alternate function mode)
  • Verified UART7 peripheral initialization is correct
  • Checked baud rate and UART settings
  • Confirmed hardware wiring:
    • External TX connected to STM32 UART7_RX
    • Common GND connected
    • Signal level is 3.3V
  • Tried disabling trace/SWO in CubeMX by setting by debug to “Serial Wire” instead of trace mode
  • Also tested with debugger disconnected after programming

My question:

  • Is the JTDO/TRACESWO pin fully usable as UART7_RX on STM32H5, or is it reserved/limited due to debug trace functionality?
  • Is there any additional register/configuration needed to release this pin from SWO/JTAG?
  • Has anyone successfully used this pin as UART RX in an STM32H5 project?

MCU part number: STM32H563RGT6
Package: LQFP64
Pin name: PB7/UART7_RX(55 num Pin)
Toolchain: STM32CubeMX / STM32CubeIDE
Debugger: ST-Link V2

Any guidance would be appreciated. Thanks!

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 12:45 PM UTC

Hello,


@Jinal wrote:

Pin name: PB7/UART7_RX(55 num Pin)


You mean PB3 not PB7.

Ok but did you disconnect the debugger probe while testing the UART? This pin is used also by the Serial Wire Debug: SWO signal.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 12:45 PM UTC

Hello,


@Jinal wrote:

Pin name: PB7/UART7_RX(55 num Pin)


You mean PB3 not PB7.

Ok but did you disconnect the debugger probe while testing the UART? This pin is used also by the Serial Wire Debug: SWO signal.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.