Skip to main content
Associate III
Mar 11, 2024 10:06 AM UTC
Question

STM32H5 I3C Target don't send ACK when receive header

My I3C target don't send ACK after controller send an arbitration header ,and it will generate a DOVER flag and ERRF flag.

 

ex.

Send HAL_I3C_Ctrl_IsDeviceI3C_Ready before controller transmit data.

Send HAL_I3C_DIRECTION_READ 

and so on

This topic has been closed for replies.

4 replies

Foued_KH
ST Employee
Mar 11, 2024 10:19 AM UTC

Hello @Sunwaz ,

Did you assign a dynamic address for the slave before starting the I3C communication ?

Let me know !
Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SunwazAuthor
Associate III
Mar 12, 2024 1:19 AM UTC

Hi @Foued_KH 

 Yes.

I can enter I3C interrupt handle.But it will generate a HAL_I3C_ERROR_DOVER or HAL_I3C_ERROR_SIZE failed.

 

 

 

void bsp_i3c_config( void ){
 aContextBuffers_Tmp.RxBuf.pBuffer = i3cRxBuffer_Tmp;
 aContextBuffers_Tmp.RxBuf.Size = sizeof(i3cRxBuffer_Tmp);
 aContextBuffers_Tmp.TxBuf.pBuffer = i3cTxBuffer_Tmp;
 aContextBuffers_Tmp.TxBuf.Size = sizeof(i3cTxBuffer_Tmp);

 aContextBuffers.RxBuf.pBuffer = i3cRxBuffer;
 aContextBuffers.RxBuf.Size = sizeof(i3cTxBuffer);
 aContextBuffers.CtrlBuf.pBuffer = i3cCtrlBuffer;
 aContextBuffers.CtrlBuf.Size = 1;

if(HAL_I3C_ActivateNotification(&hi3c1 , &aContextBuffers_Tmp , HAL_I3C_ALL_TGT_ITS) != HAL_OK){
 TARGT_DEBUG("[i3c error]start active notification failed!\r\n");
 Error_Handler();
}

if(HAL_I3C_Tgt_HotJoinReq_IT(&hi3c1) != HAL_OK){
 TARGT_DEBUG("[i3c error]enable hot join function failed!\r\n");
 Error_Handler();
 }
}

void bsp_i3c_app( void ){
if(i3c_Event & 0x01){
 if(LL_I3C_IsEnabledOwnDynAddress(hi3c1.Instance)){
 TARGT_DEBUG("[i3c event]update Dynamic Address [%d]\r\n",LL_I3C_GetOwnDynamicAddress(hi3c1.Instance));
 if(HAL_I3C_Tgt_Receive_DMA(&hi3c1, &aContextBuffers) != HAL_OK){
 TARGT_DEBUG("[i3c error]enable receive it failed!\r\n");
 Error_Handler();
 }
 i3c_Event &=~ (0x01);
 }
 }else if(i3c_Event & 0x02){
 bsp_i3c_errorHandle();
 i3c_Event &=~ 0x02;
 }else if(i3c_Event & 0x04){
 uint16_t bufferSize = LL_I3C_GetXferDataCount(hi3c1.Instance);
 if( bufferSize != 0){
 TARGT_DEBUG("[i3c event]Rx data done!Size [%d]\r\n\t[Rx]%s\r\n",bufferSize,aContextBuffers.RxBuf.pBuffer);
 memset(aContextBuffers.RxBuf.pBuffer , 0 , bufferSize);
 bsp_i3c_ProtocolParsing(aContextBuffers.RxBuf.pBuffer , bufferSize);
 }
 if(HAL_I3C_Tgt_Receive_DMA(&hi3c1, &aContextBuffers) != HAL_OK){
 TARGT_DEBUG("[i3c error]enable receive it failed!\r\n");
 Error_Handler();
 }
 i3c_Event &=~ 0X04;
 }
}

 

 

SunwazAuthor
Associate III
Mar 12, 2024 1:35 AM UTC

Sunwaz_1-1710207024718.png

When the controller send this command, the target will report HAL_I3C_ERROR_DOVER code.

SunwazAuthor
Associate III
Mar 12, 2024 1:37 AM UTC

And when the dynamic address of the target does not match,it will not respond to this command.