Skip to main content
_EFrie
Senior
Dec 17, 2025 12:58 PM UTC
Question

STM32H5 Flash layout obk and sytem

Is there a comprehensive single documentation source of the Flash layout for say, an STM32H563?

The documentation I find is very opaque.  Questions I have at present (From a non secure perspective):
1. Where is OBK located? (0x0BF0000 to 0x0BF9FFFF ???)

2. Where is system located?

3. Is RSSLIB actually using OBK memory? Or is this located somewhere else?

4. Is there a way to self program the debug password for PRODUCT_STATE > OPEN?

5. If #5 true, are there some real docs on this?  All I find so far is tutorials and code for the 573 in a secure perspective.

 

2 replies

Pavel A.
Dec 18, 2025 12:48 AM UTC

While waiting for more useful responses - click on this icon in the lower right corner

PavelA_0-1766018830454.png

ask your questions and it will search the manuals for you ))

_EFrie
_EFrieAuthor
Senior
Jan 7, 2026 10:36 PM UTC

Hmm.  I wonder if this is even an option in a NS application.

 

unsigned char * obk = (unsigned char *)FLASH_OBK_HDPL3NS_BASE_NS;

 

Basically all I can read is 0x00's , so there must be some undefined issue.  HDPL is 0 as far as I can tell.

 

Ultimately the doc's are geared toward the 573 and or TZ enabled.