Skip to main content
Associate
July 7, 2024
Question

STM32H5 Dual Differential ADC changes common mode voltage depending on clock setting

Hi guys, I'm running two differential pairs into two ADC's of an STM32H562RG. The traces are DC blocked by 47nf caps. The ADC's are setup in a master and slave dual simultaneous differential mode, running at 2 MHz each. Data is transferred by DMA. The signal of interest is a baseband signal coming from a tuner IC. The ADC's are timer triggered by TIM2.

 

VREF on the *562RG is connected to VDDA which is 2.5V (stable)

System clock (adc_hclk) is 240MHz

ADC master clock (adc_ker_ck) is 120 MHz

ADC sample time is 2.5 cycles

 

With the differential setup I'm expecting both positive and negative ADC channels to be VREF/2. This is true when I select the ADC clock setting to be "ADC_CLOCK_ASYNC_DIV4". To my knowledge this will result in a 30MHz clock coming off the ADC master clock, with 12.5 cycles + 2.5 cycles making it just in time for my 2 MHz sample rate (15 cycles at 30 MHz).

 

When probing the channels with an oscilloscope I found that the signal (data) coming from the tuner IC is a bit distorted (contains large spikes/random noise) and doesn't contain my signal of interest. This changes when I set the ADC clock source to "ADC_CLOCK_SYNC_PCLK_DIV4". Doubling the ADC clock speed. This also "pulls" the negative channel to just above VSSA and the positive channel to about VREF/2. The signal of interest re-appears on my scope. The ADC measures about 1.25V when the tuner is disabled, giving me a large default offset of about 2047 + 1023.

 

I have since then tried about every combination I could think of. More cycles per sample, reducing the main clock to as low as 120MHZ. But every time I switch from a synchonous clock to an asynchronous clock the common mode voltage changes and I can't find our why. I'm trying to keep the synchonous clock because I read the possible jitter issue from clock domain syncing.

 

I'm happy to post my code but I think I'm overlooking something obvious here. Hoping for the "aha-duh" moment in your reply. Kind regards and I appreciate any help.

This topic has been closed for replies.

1 reply

ParAvionAuthor
Associate
July 10, 2024

Update: There seems to be a relation between ADC speed, sample time and timer setup. It’s one I have yet to crack. I’ve removed the caps to isolate from the tuner IC and brought VDDA (VREF) back up to 3V3 but that doesn’t help. I’ve also switched out the MCU and connected the board to a more powerful power supply. It’s very hard to get the common voltage at VREF/2. I’ve even seen the negative channel stay idle above the positive channel by 0.1V. Running the calibration seems to have a small effect on the voltage, which also seems weird. Am I wrong to assume the common mode voltage will be supplied by the ADC or is the H5 the issue here?

 

I’m now at: changing any ADC parameter involving timing wildly affects common mode voltage. Even at very low frequencies.

 

Anyone? Suggestions as to what to try next?