Skip to main content
ca_it
Visitor II
November 26, 2024
Question

STM32G491KEU3 stuck with TrustZone on? Can read data but not write

I have just spun up some prototype boards for a project I am working on, and I am unable to program the MCU.

I am using STM32CubeProrgammer on Windows, but have also tried Linux flashing utilities such as OpenOCD. I can read data (all F) in both cases, but not erase or flash the MCU.

When attempting to connect, I can only connect if I am in "HotPlug" mode, otherwise I get an error saying "While trust zone is enabled please try connecting via HotPlug mode"

I have no idea what trustzone is but it looks like some kind of secure boot. These chips are brand new samples sent to me by ST. I reached out to ST today but haven't heard back because it is the holidays so I figured I would post here.

I checked all the option bytes but I don't think anything is set in a way that would prevent flashing, but I am also not a software developer so I'd appreciate any guidance on that.

Any ideas? Anything is helpful, even if I've tried it already in some way.

Thank you
Chase

This topic has been closed for replies.

1 reply

STOne-32
ST Technical Moderator
November 26, 2024

Dear @ca_it ,

we have no TrustZone in STM32G4 series which is based on Cortex-M4 core , TrustZone is coming with Cortex-M33 core in series such as STM32U5,L5,H5  for instance . I assume this is a generic message shown by our STM32CubeProgrammer not able to connect to the device , so most probably a hardware issue . Is that possible to share your schematics : VDDx, Boot pin , SWD pins and NRST to do a sanity check , also it may happen a soldering issue or something like. Try to boot from internal bootloader also and send us the screenshots .

Hope it helps ,

STOne-32