Skip to main content
MB.13
Associate II
Jun 20, 2025 5:37 AM UTC
Question

STM32G491 MCU Power Delivery Specification

Hi STM Team, 

 

We are planning to use STM32G491 MCU in our application. As per datasheet, it is mentioned that STM32G491 MCU will support USB PD 3.0.

 

We have come across the below STM document where it is mentioned that "STM32 UCPD MCUs are compliant with the latest USB PD r3.1 specifications" and EPR support is there.

 

Could you please confirm, whether STM32G491 MCU supports USB PD 3.1 and Extended Power Range Support(upto 240W).

 

Warm Regards,

Mythili B

 

This topic has been closed for replies.

5 replies

ST Technical Moderator
Jun 20, 2025 5:07 PM UTC

Hi @MB.13 

Yes, the STM32G491 MCU supports the USB Power Delivery (USB PD) 3.1 specification, including features like Extended Power Range (EPR) for up to 240W. However, this support is contingent on using an updated software stack, such as the X-CUBE-TCPP middleware, which implements the USB PD 3.1 standard.

Support for USB PD 3.1, including features like Extended Power Range (EPR) (up to 240W), is primarily determined by the software stack rather than the UCPD hardware itself. The USB PD 3.1 standard introduces new messaging and behaviors, such as EPR mode, which are implemented in the software stack like X-CUBE-TCPP.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
MB.13
MB.13Author
Associate II
Jun 21, 2025 1:44 AM UTC

Hi,

Thanks for your reply.

Can you also please suggest any port protection ICs like TCPP01-M12 for EPR(240W) sink applications.

We have seen in the datasheet of TCPP01-M12, where maximum voltage is 24V. But for our EPR application, max Voltage atleast protection IC should support 48V.

 

Warm Regards,

Mythili B 

MB.13
MB.13Author
Associate II
Jun 24, 2025 4:07 AM UTC

Hi,

 

Any update on this?

 

Warm Regards,

Mythili B