STM32G484 RTC LSE fails to ready, stuck waiting LSERDY, LSI works fine
Hi,
I'm using STM32G484. I need RTC to keep time after power loss, so I use external 32.768kHz LSE crystal for RTC. The program gets stuck in the waiting loop: while (READ_BIT(RCC->BDCR, RCC_BDCR_LSERDY) != 0U); It never gets LSERDY flag set.
If I switch RTC clock source to LSI, everything works normally. RTC can keep the last time value after power cycle.
Hardware info:
- 32.768kHz crystal connected to LSE_IN / LSE_OUT
-The LSE circuit uses a 32.768 kHz crystal AV25000023, with 5.6 pF load capacitors on both PC14 and PC15. The HSE is a 24 MHz crystal NX2016SA-24MHZ, which works fine. LSE fails to start and the LSERDY flag never gets set, while RTC works correctly with LSI.



-HAL library, STM32G484 - LSE is enabled in RCC BDCR register before waiting LSERDY - No debugger interference when cold power-on




Questions:
1. What possible causes make LSE fail to start on STM32G484?
2. Is there any special errata or limitation for LSE on G4 series?
3. Any recommended debug method or register check? Thanks.