STM32G474VET6 ADC2_IN5 PC4 impedance issue
- 16 replies
- 54 views
Problem with input impedance on ADC2_IN5 / PC4 / pin 30 (100pin)
I have a high speed buffer video signal from a CCD device for high speed conversion - 5 signals going to ADC1,2,3,4,5
(Our first prototype based on STM32G474RET6 used ADC1->4 - no problems with a smaller part )
Upgraded to a 100 pin part - connecting the signal to ADC2_IN5 now overloads the video signal and pulls it down - same signal behaves properly when routed to ADC1,3,4,5. No pin stacking, no input multiplexing - always converting on the same channel:
VIDEO1 - ADC3_IN3 - PE13 p44 WORKS
VIDEO2 - ADC5_IN2 - PA9 p70 WORKS
VIDEO3 – ADC4_IN4 - PB14 p53 WORKS
VIDEO4 – ADC1_IN1 - PA0 p20 WORKS
VIDEO5 – ADC2_IN5 – PC4 p30 - PROBLEMS
Signal is driver with a high speed op-amp with 50 ohm matching.
DC part of the signal attenuated as well as the AC part.