Skip to main content
Associate
Mar 13, 2026 6:47 PM UTC
Solved

Stm32g474re-nucleo FDCAN internal loop not working

Hi, I have all configured using internal loop FDCAN1 and there is not working on my STM32G474RE-Nucleo board

 

Screenshot 2026-03-13 194621.png

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 13, 2026 9:28 PM UTC

Hello,

"Not working" does mean nothing. What problem you are facing? in transmit? in receive? 

Try to use external loopback mode and monitor FDCAN_Tx pin.

I am not comfortable with setting 1Tq to the time segments. Here you are setting 1Tq for TSEG2:

screenshot.png

Try to set NTSEG1 = 17TQ and NTSEG2=2TQ

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

TDK
Mar 13, 2026 6:51 PM UTC
"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 13, 2026 9:28 PM UTC

Hello,

"Not working" does mean nothing. What problem you are facing? in transmit? in receive? 

Try to use external loopback mode and monitor FDCAN_Tx pin.

I am not comfortable with setting 1Tq to the time segments. Here you are setting 1Tq for TSEG2:

screenshot.png

Try to set NTSEG1 = 17TQ and NTSEG2=2TQ

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Karl Yamashita
Super User
Mar 13, 2026 11:00 PM UTC

Upload your IOC file. Also show some code. We don't know if you configured the filters correctly and if you even started the CAN controller with interrupts.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
mƎALLEm
ST Technical Moderator
May 20, 2026 11:05 AM UTC

Hello,

Could you please state on this thread?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.