STM32G474RE HRTIM ADC Injected Conversions not triggered
- 1 reply
- 1032 views
Hi there,
I am configuring HRTIM TIMD to generate PWM which works as expected, roughly following the Synchronous Buck Converter example for the DPOW1 eval board (my target is the nucleo64).
I use LL API calls instead of HAL calls for my project. I have configured an interrup handler to service the JEOC interrupt before calling LL_ADC_INJ_ReadConversionData12() (? - not even sure if this is correct). I do not see my interrupt handler being called so either:
a) ADC conversion is not being triggered, or,
b) ADC conversion is triggered but interrupt JEOC isn't being generated.
Can someone suggest a way of ruling out one or the other problem? For example, is there a blocking LL API call that will allow reading of completed conversions? Is there an example of this somewhere for reference?
Thanks for any help in advance.